This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM57x GPMC read access time

Other Parts Discussed in Thread: AM5728

Hi all,

We plan to interface an asynchronous memory to GPMC of AM5728. We understand that the GPMC_FCLK is same as L3_CLK which is 266MHz.

From the GPMC timing parameters, I find that maximum RDACCESSTIME / WTACCESSTIME of GPMC is 116ns (3.7593ns*31clk).
But the memory device choosen has 150ns of read/write accesstime. 

1. Is there a way the GPMC can be interfaced with this memory device of higher readacess time with the same GPMC_FCLK of 266MHz? I hope this is possible using Ready/Busy signal of memory device being connected to GPMC_WAIT signal, can you please confirm this?

2. If Ready/Busy signal is not available from the memory device, then interfacing is not possible at GPMC_FCLK of 266MHz. Then lowering GPMC_FCLK or L3 Clock (such that the readaccess time of memory device is met) is the only option. Is this correct? 

Thanks.

Regards,

Shareef