Hello,
We have an OCCB 6657 as EP, connected in a freescale board (RC ), using a powerpc processor.
we use the linux kernel 3.12.13
Either we set the the INTA or INTB in INT_PIN register at EP (c6657 ) the same interrupt is driven by PCIE in RC. Why does this happen?
Should the interrupt that fired be diffrent , when we set different legacy interrupts ?
George