Other Parts Discussed in Thread: CCSTUDIO
Greetings community!
For our Digital Signal Processors class, we've been entrusted to develop a digital transmultiplexer. This implies we need to use two cards one for the multiplexing and other for demultiplexing the signal.
The thing is, that we need to synchronize both cards. For instance, we decided to use an external interrupt.
First, we'll turn on the receiver. It will keep on an infinite loop until it receives the external interrupt from the emitter, so it starts saving the received samples from the CODEC to process them and separate the signals. The algorithm was developed to support N channels, but due to the hardware limitations (mainly CODEC channels and CODEC sample rate, it was limited to 4 channels). We put a signal on the first ("0") channel via a microphone and receive via the same channel on the other side of the system.
The past week we succesfully tested the emitter and the receiver by separate, now we got to sync them. We will be able to test our sync method next monday.
So, as a quick-n-dirty solution we're using the EMIF port at the emitter to generate the transition needed for the interrupt (first putting it in an 0 to 1 or viceversa).
To receive the interrupt, we're using the EXT_INT4 pin on the J3 peripheral interface at the receiver card. It's connected via de GPIO, and we've already put the HPI_EN pin to the pull-down resistor via the dipswitch described HERE.
We've checked this great forum, with topics such as:
GPIO Hardware Interrupts Question
And read these docs:
* spru584a - TMS320C6000 General Purpose I/O Reference Guide
* spru646a - TMS320C6000 DSP Interrupt Selector Reference Guide
* TMS320C6713 Datasheet
* DSK6713 Technical Reference
* C6713 Chip Support Library Guide
* spru733a - C67xx CPU and Instruction Set Guide (chapter 5 - Interrupts)
We're running on C6713 Code Composer Platinum v3.1 Note that we added all neccesary libraries (dsk init, dsk6713.cmd, bsl, csl... aic23, led...)
To test this, i made a simple program that would receive that interrupt turning on a LED and changing a flag value. I based it on what others have done in the mentioned forum threads.
First of all, our basic code to test if the interrupt is actually being processed:
// TMXReceptor.c // IRQ test version
/* // TMXReceptor.c
UPIITA-IPN
David VP
Program used to test external interrupts
*/
// dsk6713_led.h and others are added to the project via code composer
#include "C:\CCStudio_v3.1\C6000\dsk6713\include\dsk6713_aic23.h"
Uint32 fs=DSK6713_AIC23_FREQ_32KHZ; // Tasa de muestreo CODEC
#include "C:\CCStudio_v3.1\C6000\dsk6713\include\dsk6713.h"
#include <stdio.h>
// #include <string.h>
#include <stdlib.h>
#include <math.h>
#include <time.h>
#include <csl_gpio.h>
#include <csl_gpiohal.h>
#include <csl_irq.h>
#include "db4_2etapas.h"
// M, N and sinc are defined in "db4_2etapas.h" apart from filters' coefficients.
// Global Variables (Variables globales)
int flag = 1;
int iter = 0;
int startflag = 0;
int outputflag = 0;
float abuffer[N] = {0}; // Buffer para recuperacion
GPIO_Handle gpio_handle; /* handle para el GPIO - GPIO Handle*/
//Configuración de los registros del GPIO (GPIO Registers' Configuration)
GPIO_Config gpio_config = {
0x00000000, // gpgc = Modo Passthrough de Interrupciones y control directo sobre GP0
// Passthrough Interruption mode and direct control over GP0
0x0000FFFF, // gpen = Todos los pines de GPIO de 0 a 15 habilitados
// All GPIO pins enabled (from 0 to 15)
0x00000000, // gdir = Todos los pines de GPIO como entradas
// All pins as inputs
0x00000000, // gpval = Guarda el nivel lógico de los pines
// Record logic level of the pins
0x00000010, // Activar IRQ para pin 4
// Enable IRQ at pin 5
0x00000010, // Activar evento de irq para pin 4
// Enable pin 4 EDMA irq event
0x00000000 // gppol -- default state
// Default - Rising edge
};
// This can be written to a separate .c file
irq_ext_enable(){
// First, globally disable interrupts
// CSR [Control Status Register] Bit 0 is GIE [Global Interrupt Enable]
// Set last bit to ZERO
CSR = (CSR)&(0xFFFFFFFE);
// Set the NMIE bit (bit #1) at the IER
IER |= 0x00000002;
// Set the INT4 bit (bit #4) at the IER
IER |= 0x00000010;
// Last, globally enable interrupts (CSR last bit to 1)
CSR |= 0x00000001;
}
main()
{
// Configure GPIO
gpio_handle = GPIO_open( GPIO_DEV0, GPIO_OPEN_RESET );
GPIO_config(gpio_handle,&gpio_config);
// ENABLE EXTERNAL INTERRUPTS
irq_ext_enable();
comm_intr(); //init DSK, codec, McBSP
DSK6713_LED_init();
while(startflag == 0); // esperar a la sincronización del otro DSP
while(1)
{
while(flag == 1); // Wait for the CODEC interrupt to clear the flag
if(iter > sinc) outputflag = 1; // Wait for #[sinc] samples then output the results
// ###################################################
// ALL THE ALGORITHM IS PUT HERE
// ####################################################
} // End of infinite while (Fin del while infinito)
} //end of main
interrupt void c_int04() //ISR INT_EXT4
{
startflag = 1; // Turn on the main program's flag
iter = 0; // Reset the iteration counter
DSK6713_LED_on(0); // Turn on the led
}
interrupt void c_int11() //ISR
{
inputbuffer = (float)((short)input_sample()); // Get a sample
if(outputflag == 1) // If the interrupt was already received, output samples
{
output_sample((short)(outputbuffer)); // Output recovered signal
}
else // otherwise, output zeros
{
output_sample((short)(0)); // Output zero sample
}
flag = 0; //set flag to resume algorithm flow
}
// TMXReceptor.c End of File
After that, we've modified our vectors_intr.asm (got it from the book) just adding the details for the ext interrupt 4 to get handled by a function in our C code. It looks like this:
<<< File begins after this line >>>
*Vectors_intr.asm Vector file for interrupt INT11
.global _vectors ;global symbols
.global _c_int00
.global _vector1
.global _vector2
.global _vector3
.global _c_int04 ; symbol for EXT_INT4
.global _vector5
.global _vector6
.global _vector7
.global _vector8
.global _vector9
.global _vector10
.global _c_int11 ;for INT11
.global _vector12
.global _vector13
.global _vector14
.global _vector15
.ref _c_int00 ;entry address
VEC_ENTRY .macro addr ;macro for ISR
STW B0,*--B15
MVKL addr,B0
MVKH addr,B0
B B0
LDW *B15++,B0
NOP 2
NOP
NOP
.endm
_vec_dummy:
B B3
NOP 5
.sect ".vecs" ;aligned IST section
.align 1024
_vectors:
_vector0: VEC_ENTRY _c_int00 ;RESET
_vector1: VEC_ENTRY _vec_dummy ;NMI
_vector2: VEC_ENTRY _vec_dummy ;RSVD
_vector3: VEC_ENTRY _vec_dummy
_vector4: VEC_ENTRY _c_int04 ;INT04 Ext
_vector5: VEC_ENTRY _vec_dummy
_vector6: VEC_ENTRY _vec_dummy
_vector7: VEC_ENTRY _vec_dummy
_vector8: VEC_ENTRY _vec_dummy
_vector9: VEC_ENTRY _vec_dummy
_vector10: VEC_ENTRY _vec_dummy
_vector11: VEC_ENTRY _c_int11 ;ISR address
_vector12: VEC_ENTRY _vec_dummy
_vector13: VEC_ENTRY _vec_dummy
_vector14: VEC_ENTRY _vec_dummy
_vector15: VEC_ENTRY _vec_dummy
<<< File ends the line before >>>
Is there anything I've missed? I've enabled the interrupt individually, I've enabled the GPIO pin and configured it as an interrupt, also set up the interrupt in the vectors_intr.asm file. The program gets compiled with no errors or warnings.
I'll be grateful for any advice!
- David