I am Using RTOS on DM8148 , I am trying to display an image from A8 to M3. A8 is placing the data in memory while M3 is reading from that Location and displaying it . The problem is the image doesnt show up completely there are empty line in between . When i am running my function two or three times i can see the complete image. I am using AVSDK package for DM8148
While running it without RTOS i am getting a very slow processing speed, but i am getting a whole frame in running the function single time.Please help me with this.
BR
AMMAR