This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138, TMS320C6748 Documentation errata PINMUX10, PINMUX11, PRU1_R31[18-23]



It is unclear which functions are multiplexed with PRU1_R31[18-23], and the corresponding pins.

For example, as regards PRU1_R31[18], in the datasheets

OMAP-L138 Low-Power Applications Processor (Rev. A)

TMS320C6748 Fixed/Floating Point Digital Signal Processor (Rev. A)

(Figure 3-5 and Table 3-11),

PRU1_R31[18]  is multiplexed with EMA_A[18]:

EMA_A[18] / MMCSD0_DAT[3] / PRU1_R30[26] / GP4[2] / PRU1_R31[18].

However in

OMAP-L138 Applications Processor System Reference Guide (Rev. D)

TMS320C6748 DSP System Reference Guide (Rev. D)

OMAP-L1x8, TMS320C6742/6/8 Pin Multiplexing Utility (Rev. B)

a different multiplexing is reported (see Table 11-33):

PRU1_R31[18]/EMA_A[10]/PRU1_R30[18]/GP5[10].

It seems that the relevant PINMUX registers are not affected, because the PRU1_R31 functions are selected by  the value 0.

I can't probe these pins right now. So which information is true?