HI!
I am trying to config pins for SPI0 - CS1 (ICE v1) and don't undestand what I am doing wrong.
There is my code:
#include <xdc/std.h> #include <ctype.h> #include <string.h> #include <xdc/runtime/System.h> #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/family/arm/a8/intcps/Hwi.h> #include "stdlib.h" #include "soc_AM335x.h" #include "plat_utils.h" #include "osdrv_uart.h" #include "osdrv_mmu.h" #include "osdrv_version.h" #include "osdrv_oledlcd.h" #include "osdrv_mcspi.h" #include "plat_mux.h" unsigned char uartInstance = 0; unsigned char boardType = 0;
MUX_CONFIG mux[] = {
{ 0x0950 , 0 , AM335X_PIN_OUTPUT | AM335X_PIN_INPUT }, // spi0_sclk
{ 0x0954 , 0 , AM335X_PIN_INPUT }, // spi0_DO
{ 0x0958 , 0 , AM335X_PIN_OUTPUT }, // spi0_DI
{ 0x095C , 0 , AM335X_PIN_OUTPUT| AM335X_PIN_INPUT_PULLUP }, // spi0_cs0
{0xFFFFFFFF,0,0}
};
SYS_MMU_ENTRY applMmuEntries[] = {
{(void*)0x48300000,0}, //PWM - Non bufferable| Non Cacheable
{(void*)0x48200000,0}, //INTCPS,MPUSS - Non bufferable| Non Cacheable
{(void*)0x48100000,0}, //I2C2,McSPI1,UART3,UART4,UART5, GPIO2,GPIO3,MMC1 - Non bufferable| Non Cacheable
{(void*)0x48000000,0}, //UART1,UART2,I2C1,McSPI0,McASP0 CFG,McASP1 CFG,DMTIMER,GPIO1 -Non bufferable| Non Cacheable
{(void*)0x44E00000,0}, //Clock Module, PRM, GPIO0, UART0, I2C0, - Non bufferable| Non Cacheable
{(void*)0x4A300000,0}, //PRUSS1 - Non bufferable| Non Cacheable
{(void*)0x49000000,0}, //EDMA3 - Non bufferable| Non Cacheable
{(void*)0x4A100000,0}, //CPSW - Non bufferable| Non Cacheable
{(void*)0xFFFFFFFF,0xFFFFFFFF}
};
/* ======== main ========
*/
Void main()
{
Task_Params taskParams;
MMUInit(applMmuEntries);
boardType = UTILsDetectBoardType();
if(AM335X_BOARD_TYPE_ICE == boardType)
{
uartInstance = 5;
}else if(AM335X_BOARD_TYPE_IDK == boardType)
{
uartInstance = 3;
}
else if( AM335X_BOARD_TYPE_ICE_V2 == boardType)
{
uartInstance = 3;
}
PinMuxConfig(mux);
McSPIInit(MCSPI_INSTANCE_0, 12, 1 , MCSPI_SINGLE_CH, MCSPI_CHANNEL_0);
while (1) {
unsigned char *charbuff;
unsigned char x = 173;
charbuff = &x;
McSPIWrite(1, &charbuff, 8, 0);
}
}