Other Parts Discussed in Thread: TMS320VC5505
Hi,
Sorry if this is a rhetorical question, however I am currently evaluating a SEED XDS560 PLUS emulator and also an XDS510USB with a custom board using a TMS320VC5505, that we have developed on the XDS100.
However when configuring using CCS Setup 3.3 I am having trouble locating the correct GEL file for the c5505 that configures CCS correctly for the above emulators ?!? Is there one GEL file for each of the above emulators that covers several DSPs or one specific for the C5505 & C5515 ??
At first glance it appears that for the C55XX family only the C5502 / C5509 / C5510 / C5561 are actually supported by the CCS Setup 3.3. Would these be supplied by the emulator manufacturers or are they available elsewhere ?? Any info would be greatly appreciated.
Thanks in advance,
M MARIN