Hi
Hardware Design Guide says:
6.2.5 Unused HyperLink Pin Requirement
If unused, the primary HyperLink clock input must be configured as indicated in Section 3.3, Figure 15. Pull-up must be to the CVDD core supply
However, in the same document, Table 8 Managing Unused Clock Inputs says it should be left floating.
Which is correct pin requirement ?
Best Regards,
Naoki