This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6746 Deep Sleep current drain

Hi

In the application I am working with (single C6746), the current drain was measured at 50mA during deep sleep.  In previous applications using a C55, the same current was measured at 25mA.  My questions are:

1- Is the C6746 expected to have a current similar drain as the C55 during deep sleep?

2- Do you have information about this expected current drain/power during deep sleep mode for the C6746?

Thanks