This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X DMTIMER PWM single pulse duration - prescaler?

Hi everyone,

Quick question regarding the interpretation of this statement:

AM335X TRM 20.1.3.1 Timer Mode Functionality:

" A dedicated output pin (PORTIMERPWM) is programmed through TCLR (TRG and PT bits) to generate one positive pulse (prescaler duration)"

Unfortunately I have no scope to hand so I'm not able to visually verify this, so I have to ask: in pulse mode, does this mean that the prescaler value controls the PWM pulse duration even if prescaler itself is not enabled, or does it simply mean that the PWM pulse is always one cycle long, thus longer if prescaler is used?

In my current project I'm generating a pulse per second (1PPS) signal using the PWM, and I need to be able to control the pulse duration: if the prescaler controls it, I will use pulse mode and prescaler, but if not, I will need to use toggle mode with overflow and match to control the pulse.

Thanks,

Wojciech