We are in the process of moving from the last sitara sdk (8 I believe) to the latest TI Processor SDK (2.00.1). We use the omap_uart (omap-serial?) driver to automatically handle the 485 half duplex control. Back in the old sitara sdk this worked with serial formats 8N1 and 7E2, but in the latest sdk we only see 8N1 function and not the even parity. The normal RS232 port still works fine for both formats, so it seems to be specific to the 485 function. Was a bug introduced into this driver or am I overlooking something?