Other Parts Discussed in Thread: ADS1220
Hi,
I am trying to establish communication with the external ADC, ADS1220, and I am using the CSL_spi_internalLB example coupled with trying to implement the psuedo code recommended in the adc's datasheet. I have two main questions. The pseudo code recommends to assert the CS to high and low at different points in the code and I am not sure how to do that in the DSP. Is that the same idea as the spi_Open function? Additionally, I'm unsure of how to check for when DRDY transitions to low, or send the 24 sclk rising edges to read out conversion data on DOUT/DRDY.
Below is my code that is attempting to interface and communicate with the ADC. It currently just shows that in the read buffer old configurations that I wrote to the write buffer. Any advice is appreciated and it would also be nice to know if I am moving in the write path as far as the code goes or going in the wrong direction. Thank you in advance.
Best Regards,
Ulbert
#include "csl_spi.h"
#include "csl_general.h"
#include "cslr_spi_001.h"
#include "corazon.h"
#include "ezdsp5535.h"
#include <stdio.h>
#define CSL_TEST_FAILED (1)
#define CSL_TEST_PASSED (0)
#define CSL_SPI_BUF_LEN (1)//(64)
#define SPI_CLK_DIV (24)
#define SPI_FRAME_LENGTH (1)
Uint16 spiWriteBuff[CSL_SPI_BUF_LEN];
Uint16 spiReadBuff[CSL_SPI_BUF_LEN];
Int16 spi_sample(void)
{
Int16 status = CSL_TEST_PASSED;
Int16 result;
CSL_SpiHandle hSpi;
SPI_Config hwConfig;
volatile Uint32 looper;
result = SPI_init();
if(CSL_SOK != result)
{
status = CSL_TEST_FAILED;
return (status);
}
else
{
printf ("SPI Instance Initialize successfully\n");
}
//see if this is the equivalent of asserting the CS
hSpi = SPI_open(SPI_CS_NUM_1, SPI_POLLING_MODE);
if(NULL == hSpi)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Opened successfully\n");
}
/** Set the hardware configuration */
hwConfig.spiClkDiv = SPI_CLK_DIV;
hwConfig.wLen = SPI_WORD_LENGTH_8;
hwConfig.frLen = SPI_FRAME_LENGTH;
hwConfig.wcEnable = SPI_WORD_IRQ_DISABLE;
hwConfig.fcEnable = SPI_FRAME_IRQ_DISABLE;
hwConfig.csNum = SPI_CS_NUM_1;
hwConfig.dataDelay = SPI_DATA_DLY_0;
hwConfig.csPol = SPI_CSP_ACTIVE_LOW;
hwConfig.clkPol = SPI_CLKP_LOW_AT_IDLE;
hwConfig.clkPh = SPI_CLK_PH_RISE_EDGE; //was falling edge
result = SPI_config(hSpi, &hwConfig);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Configured successfully\n");
}
/*Enable the Internal Loopback mode*/
#if (defined(CHIP_C5517))
CSL_FINST(CSL_SPI_REGS->SPIDCRU,SPI_SPIDCRU_LPBK,ENABLE);
#else
#if (defined(CHIP_C5505_C5515) || defined(CHIP_C5504_C5514))
CSL_FINST(CSL_SPI_REGS->SPIDC2,SPI_SPIDC2_LPBK,ENABLE);
#endif
#endif
for(looper = 0; looper < CSL_SPI_BUF_LEN; )
{
spiWriteBuff[looper] = 0;
if(CSL_SPI_BUF_LEN>1){
spiWriteBuff[(looper + 1)] = 0;
spiReadBuff[(looper + 1)] = 0;
}
spiReadBuff[looper] = 0;
//spiReadBuff[(looper + 1)] = 0;
looper += 2;
}
//send reset command (0x06h)
// spiWriteBuff[7] = 0;
// spiWriteBuff[6] = 0;
// spiWriteBuff[5] = 0;
// spiWriteBuff[4] = 0;
// spiWriteBuff[3] = 0;
// spiWriteBuff[2] = 1;
// spiWriteBuff[1] = 1;
// spiWriteBuff[0] = 0;
spiWriteBuff[0] = 0x0006;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
EZDSP5535_waitusec(10000);
//send write reg command
spiWriteBuff[0] = 0x0040; //write to register 0, 1byte(8bits), (0100 0000)
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//config first buffer
// spiWriteBuff[7] = 1; //config the input to be AIN1 and negative reference to be tied to ground
// spiWriteBuff[6] = 0;
// spiWriteBuff[5] = 0;
// spiWriteBuff[4] = 1;
// spiWriteBuff[3] = 0;//config the gain to be one
// spiWriteBuff[2] = 0;
// spiWriteBuff[1] = 0;
// spiWriteBuff[0] = 1;//disable PGA
spiWriteBuff[0] = 0x0090;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//send write reg command
spiWriteBuff[0] = 0x0044; //write to register 1, 1byte(8bits), (0100 0100)
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//config second buffer
// spiWriteBuff[7] = 1; //config the sampling frequency to 330 sps duty cycle
// spiWriteBuff[6] = 1;
// spiWriteBuff[5] = 0;
// spiWriteBuff[4] = 0; //set to duty cycle sampling mode
// spiWriteBuff[3] = 1;
// spiWriteBuff[2] = 1; //set for continuous conversion mode
// spiWriteBuff[1] = 0; //disable temp converter
// spiWriteBuff[0] = 0; //disable burnout current sensor
spiWriteBuff[0] = 0x00CC;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//send write reg command
spiWriteBuff[0] = 0x0048; //write to register 0, 1byte(8bits), (0100 1000)
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//config third buffer
// spiWriteBuff[7] = 1; //config analog supply as voltage reference
// spiWriteBuff[6] = 1;
// spiWriteBuff[5] = 1; //config for 60Hz rejection filtering
// spiWriteBuff[4] = 1;
// spiWriteBuff[3] = 0;//config default
// spiWriteBuff[2] = 0;//config for default
// spiWriteBuff[1] = 0;
// spiWriteBuff[0] = 0;
spiWriteBuff[0] = 0x00F0;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//send write reg command
spiWriteBuff[0] = 0x004C; //write to register 0, 1byte(8bits), (0100 1100)
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//config fourth buffer
// spiWriteBuff[7] = 0; //config default
// spiWriteBuff[6] = 0;
// spiWriteBuff[5] = 0;
// spiWriteBuff[4] = 0;//default
// spiWriteBuff[3] = 0;
// spiWriteBuff[2] = 0;
// spiWriteBuff[1] = 1;//set DREADY/DOUT when data is ready
// spiWriteBuff[0] = 0;//reserved
spiWriteBuff[0] = 0x0001;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
//optional sanity check to read back all registers with RREG cmd(0x23h)
// spiWriteBuff[7] = 0; //not sure if to write to spi or read from spi
// spiWriteBuff[6] = 0;
// spiWriteBuff[5] = 1;
// spiWriteBuff[4] = 0;
// spiWriteBuff[3] = 0;
// spiWriteBuff[2] = 0;
// spiWriteBuff[1] = 1;
// spiWriteBuff[0] = 1;
// spiWriteBuff[0] = 0x0023;
// /* Write the Data to the SPI*/
// result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
// if(CSL_SOK != result)
// {
// return (CSL_TEST_FAILED);
// }
// else
// {
// printf ("SPI Instance Write successfully\n");
// }
//send start command (0x08h)
// spiWriteBuff[7] = 0;
// spiWriteBuff[6] = 0;
// spiWriteBuff[5] = 0;
// spiWriteBuff[4] = 0;
// spiWriteBuff[3] = 1;
// spiWriteBuff[2] = 0;
// spiWriteBuff[1] = 0;
// spiWriteBuff[0] = 0;
spiWriteBuff[0] = 0x0008;
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
EZDSP5535_waitusec(100);
while(1){
//send read data command
spiWriteBuff[0] = 0x0010; //write to register 0, 1byte(8bits), (0001 0000)
/* Write the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Write successfully\n");
}
/* Read the Data to the SPI*/
result = SPI_dataTransaction(hSpi ,spiReadBuff, CSL_SPI_BUF_LEN, SPI_READ);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Read successfully\n");
}
printf("readBuff = %04x\n", spiReadBuff[0]);
}
result = SPI_close(hSpi);
if(CSL_SOK != result)
{
return (CSL_TEST_FAILED);
}
else
{
printf ("SPI Instance Close successfully\n");
}
/* Compare the Data */
for( looper = 0 ; looper < CSL_SPI_BUF_LEN ; looper++ )
{
if(spiWriteBuff[looper] != spiReadBuff[looper] )
{
return (CSL_TEST_FAILED);
}
}
return (status);
}