This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 RS-232 problem

Hello Team,

One of my customer is working on DM6437. They are tring to get the video out over RS-232. What they did is that they used our examples C:\dvsdk_1_01_00_15\psp_1_00_02_00\pspdrivers\drivers\uart”  and transmit two conts integer to test the code, but eventough they are working at 25 Hz, they can only  trasmit the data 6 or 7Hz data rate. What they want to learn is why the trasmit rate is decreasing to 6 or 7 hz and also if we have any aplication code which shows the video perfromance over RS-232?

Many thanks for your support.

Best Regards

Yunus