This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build Errors while making Nk.bin



Hello

 

While am running to make run time image am getting these errors.

 

This is the error mess am getting while i trying to build my win ce.

BUILD: [01:0000000156:INFO  ] makefile.def: Including C:\WINCE600\public\
common\oak\misc\Sources.default
BUILD: [01:0000000157:INFO  ] makefile.def: BUILDROOT is C:\WINCE600\PLATFORM\
COMMON
BUILD: [01:0000000158:INFO  ] makefile.def: Including C:\WINCE600\PLATFORM\
COMMON\sources.cmn
BUILD: [01:0000000159:ERRORE] C:\WINCE600\public\common\oak\misc\makefile.def
(156) :  U1023: syntax error in expression
BUILD: [01:0000000160:INFO  ] Stop.
BUILD: [01:0000000161:ERRORE] NMAKE.EXE WinceTargetFile0  -i -c BUILDMSG=Stop.
BUILDROOT=C:\WINCE600\PLATFORM\COMMON CLEANBUILD=1 NOLINK=1 PASS0ONLY=1
failed - rc = 2

Can any body tell these are the lines in makefile.def:

                  154    # Include the developer supplied file that defines the TARGETNAME,
LINE NO: 155   # TARGETTYPE and SOURCES macros.
LINE 156:          #
        158              # Local variable which gets set to the tree being
built currently
         159               WINCETREE=$(_CURSLMTREE)

can any body tel what to correct in these..

 

 

Regards

Vinoth.