Hi all,
I recently had a problem with the function atan2sp which wasn't giving me the expected result. It was a kind of multiplied by two. I then replaced it with the atansp, passing it the quotient of the input values. The result was right.
Did anyone had similar problems with the atan2sp or atan2dp ? Is this the right behaviour ?
I run it on a C6657, using CCSv6 and the compiler c6000_7.4.15, set in floating point strict mode.
Thanks,
Luca