This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ethernet problem on c6678 custom board



hello

after some test with evmc6678, we switched into our custom board. on emvc6678, we used CCS and load "c6x-linux" in nfs mode, after that we program evm NAND flash and EEPROM and etc. our custom board has same schematic as evm in most part of it but the same process won't work for it.

we boot linux on initRAM mode by use of CCS and after that we found out our ethernet is not working and that was reason for "nfs boot" failure, we also checked clock source of PASS PLL and it seem to be same as evm.

is there anything we are missing is our config? because the only parameter we changed in GEL file was DDR3 and main PLL(pass pll recieve 100MHz clock similar to evm), is there something else that we should change?

question 2:

and another question is about IBL, if I program EEPROM and NAND Flash and set boot PIN correctly, will I be able to boot linux? or the FPGA on EVM is doing something behind the curtain that i should implement on our FPGA too?