Hi,
I'm Designing a board using TMS320C5515 DSP where in I'm planning to use 24 Bit SPI serial Flash to load my application program and boot from it. Is there a programmer available using which I can program the 24 bit SPI flash. The available programmer for C5515 EVM doesn't have the 24 Bit SPI programming functionality. I have tried different programmers like C5535 eZDSP etc but to no avail.
To test this feature I have replaced the SPI EEPROM on the C5515EVM board with a dropin replacement SPI Flash from Spansion.
Regards
Supreeth