Hi,
Cs0 of Dm3730 is connected to nor-flash by configuring 16-Bit Address/Data Muxed mode and cs4 of dm3730 is connected to one device that has 8-bit data and 5-bit Address. How will we connect to A0 pin of this device to Dm3730 ?
Thanks
İlker KAYA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Cs0 of Dm3730 is connected to nor-flash by configuring 16-Bit Address/Data Muxed mode and cs4 of dm3730 is connected to one device that has 8-bit data and 5-bit Address. How will we connect to A0 pin of this device to Dm3730 ?
Thanks
İlker KAYA
Hi,
Thanks for your reply.
There is no connection for 8-Bit Address/Data Muxed pSRAM or NOR Flash. Does Dm3730 support 8-Bit Address/Data Muxed mode?
Thanks.
Thanks for your reply.
After booting, If we access one component that has 8 bit datas and addresses by configuring CS4 for “8-Bit Address/Data Muxed mode” or “8-Bit Address/Data non-Muxed mode”, Can we get the address_0 value ? in other word, How will we connect to A0 pin of this device to Dm3730 ?
BR
ilker
Hi,
I tried the access. When the access is done, the related address pins of DM3730 is measured by scope. The address pins are changed like below but there is no value of zeroth bit.
DM3730 DM3730_Pin
Address A5A4A3A2A1
0x00 00000
0X01 00000
0X02 00001
0X03 00001
0X04 00010
0X05 00010
0X06 00011