Other Parts Discussed in Thread: 66AK2L06, TMDXEVMPCI, SYSBIOS, 66AK2H06, 66AK2E05
Hello,
I'm using Evaluation Module for the 66AK2L06 (the TI PN: XEVMK2LX)
Trying to activate and testing PCIe interface using test program from CCS6 for K2L.
Initialization program reports "PCIe Serdes Mux Not Selected". I checked DEVSTAT
register value, bit28 is really "0" This bit must be set to "1" if GPIO16 pin is "1" during reset.
In fact on the evaluation board XEVMK2LX there is no jumper or another simple way to set
GPIO16 to 1. How to handle this situation?
If I want to test the board's PCIe with PC there is no adaptor card AMC to PCIe which
fit the shape and size of my EVM. I mean adaptor card like TMDXEVMPCI for C6670.