Does one $ 2000 TI Blaze sEVM 4430 with Pico with HDMI 1.3 output 30-bit; output 720p of Citrix Receiver for Android running Windows Server 2008 R2 to one $ 2500 eMagin SXGA OLED-XL™' microdisplay connected to one SXGA-1012SD video driver board for a eMagin SXGA OLED-XL™ microdisplay with HDMI 1.3 input 30-bit. Does it? If it does I buy one TI Blaze sEVM 4430 with Pico instantly. Is Android' Citrix Receiver output: MPEG4 ASP, MPEG-2 MP, H.264 HP, ON2 VP7 or VC-1 AP? In other words can Citrix Receiver be controlled via the tpd12s015 or wuxga display controller serial - parallel as shown on the chip block diagram > http://focus.ti.com/en/graphics/wtbu/OMAP4430_zoom.jpg?imageURL=OMAP4430_zoom.jpg&genericPN=TMS320DM642&isFunctional=Y&isFunctional=Y Less technical: The TI Blaze sEVM4430 with Pico has HDMI output, runs android 2.1. But in the video www.youtube.com/watch you can't see if you can browse, navigate on a screen connected to the HDMI 1.3 output of the TI Blaze. PS: I saw android 2.1 - which runs on the TI Blaze sEVM 4430 with pico - on HDMI 720p on the Beagleboard www.youtube.com/watch. yours sincerely, Ivo Westerneng