Other Parts Discussed in Thread: OMAPL138
Hi,
I am trying to generate an SPI1 bootloader for my OMAP L138 Logic PD Experimenter kit. I want to generate a bootloader for the C6748 only as I am not using the ARM. I am using the serial flasher utility to flash the board. I was able to flash an example image (OMAPL138-DSP-LED-NAND-SPI-UART.bin) which I downloaded and it booted up in SPI1 master boot mode and flashed LEDs. When I try to generate my own boot image using the .out file, it will not boot. I've attached my AISGen cfg file.. could you tell me what I have missed in this cfg file?
Thanks
Brian