Hello,
We have systems which run for some time, and suddenly the stop sometimes in ubl, at other times in u-boot.
We suspect that it is a nand issue.
Does it points to that ?
We want the minimum change.
I am familiar with 2 changes, but rather do minimum changes because there are many boards spread out there.
1. we use old ubl 1.5 and there was some allignment fix in ubl 1.6.5
2. change of ecc layout in u-boot/kernel
Does the problem I described fit the fix number (1) or does it required fix number (2) ?
Regards,
Ran