Do the edge connection problems carry forward to the 5515 ezdsp.
I cannot find a picture of the ezdsp 5516 is there a reason they dont show a form picture?
Martin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do the edge connection problems carry forward to the 5515 ezdsp.
I cannot find a picture of the ezdsp 5516 is there a reason they dont show a form picture?
Martin
The details on the Edge Connector for the C5515 eZdsp are available from the Spectrum Digital support page for this product (http://support.spectrumdigital.com/boards/usbstk5515/reva/). Look in the Technical Reference document.
Regards.
MikeH,
My post was in response to original question from Martin. I hit the wrong reply button.
To the best of my knowledge there aren't any problems with the edge connector for the C5515 eZdsp. There was a problem with the original VC5505 eZdsp in that the connector used did not match the specified mating connector. A work around was developed. Here is a post on the issue: http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/110/p/11128/43310.aspx#43310.
Regards.