This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6654 EMIF NOR Boot, which section need to be loaded?

Guru 15520 points

Hi,

I have question about C6654 EMIF NOR Boot.

I understand that secondary boot loader which copies application image from NOR Flash to RAM
are need it. I guess there are no secondary boot loader provided from TI so that user need to make it.

I want to know which section need to be loaded from NOR to RAM by secondary boot loader.
Is it only ".text" and ".cinit"?

In our program, CSL are used for interrupt.
In CSL there are ".csl_vector" section. Do I also need to load this ".csl_vector" from NOR to RAM?

best regards,
g.f.