Hi! I'm trying to setup OSD Window 0 in the Video Back End of the DM369 processor. But I don't see any presense of the window on the display. Video windows 0 and 1 are configured and displayed normally. Here is my settings for the OSD window 0:
OSDWIN0XP = 384; // window start position OSDWIN0YP = 384; // window start position OSDWIN0XL = 256; // window width OSDWIN0YL = 256; // window height OSDWIN0OFST = 256 / 16; // BMPMDE = 1, input mode = YCbCr data, blending ratio = 7, frame mode, window is active (displayed): OSDWIN0MD = ((0x01 << 15) | (0x03 << 13) | (0x07 << 3) | (0x01 << 1) | (0x01 << 0));
Also the address of buffer with picture is configured in OSDWIN0OFST, OSDWINADH and OSDWIN0ADL registers.