This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what is the maximum space of DM814x FLASH

Hi Guys,

Please help to confirm the maximum FLASH can be supported for DM8148

I saw below information about GPMC:

-- 512M-Byte Total Address Space Divided Among up to 8 Chip Selects

So I guess the maximum FLASH size supported should be 512M Byte, not the 512*8(Chip Selects) = 4G Bytes?

Regards,

Miranda