I am using the TI AM335X-EVMSK with TI processors SDK 2.00.01. I have built an image using default configurations. I was able to launch the matrix browser and confirm that touch was working adequately.
I then disconnected the screen and attached an 800x480 panel. This panel is also resistive. I modified the panel timings to support this screen. I booted the EVM and the screen turned on appropriately the tslib calibration tool screen came up and I was able to calibrate the screen. The matrix browser launched and the touch pointed were off from the calibration. I launched the ts_test tool and saw that my calibration till appeared correct. I also launched the fingerpaint example included in the qt library and saw that it was off as well.
I assumed that redoing the calibration was allow the qt application to track properly is this not the case? Do you have any suggestions on how to resolve this issue?
Regards,
Matt Minga