Other Parts Discussed in Thread: SYSBIOS
Hi;
Running Win 7 64 bit here. Have the AM437x IDK. Trying to install the SYSBIOS v6.42. Following the install I get the pop up telling me that the process may not have run properly. But no clues. Moving forward I attempted to compile the EnDat diagnostic example. First I setup the configuration as per the directions to use the correct target, (EVMAM437x) and the XDS100v2 USB Debug Probe. Also bypassed the M3_Wakeup_SS_1. When I run the test I get the 'JTAG DR Integrity scan test succeeded' message . Upon attempting to compile for debug, I get an problem listing telling me that my SYSBIOS isn't installed. Yet when I check the Windows CP, the listing for the SYSBIOS is there waiting for me to uninstall? The version there is 2.1.1.2 with no size given.
Some things that may be incorrect:
Not sure I installed the GNU compiler when I ran the CCS install.
I also get a warning that my XDC\packages directory can't be found.
Any help appreciated.
Aaron