Dear TI
on the BBB the DDR3(MT47H128M16RT-25E:C 96 pin ball) schematics pin M7 is assigned as Address15 but datasheet says it is NC(Not connected)
is it correct to say M7 pin as A15
Regards
Nick

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
thanks guys this DDR3 RAM used in beaglebone minimum order quantiy is 1000 from most of the distributor hence i have decided to use IS43TR16256AL-125KBLI bellow is datasheet link

i wanted to know
Regards
Nick King said:in terms of software can you please let me know which file needs to be modified
The timings get utilized in u-boot/board/ti/am335x/board.c. Look for the call to config_ddr() in that function. There's a struct pointer passed to that function. The corresponding structure contains the timings.
Nick King said:what are the correct timings for this new chip IS43TR16256AL-125KBLI it would be great if you can send us the modified file to be used
Use the DDR calculation tool from this page:
http://processors.wiki.ti.com/index.php/AM335x_EMIF_Configuration_tips
That will get you the 3 timing registers. The rest of the wiki page has info pertaining to the rest of the registers.
And as I mentioned previously, you'll need to re-run software leveling: