Other Parts Discussed in Thread: SYSBIOS
Dear Champ,
My customer is trying to developing 'monitoring system' to check CPU load continually in the field by sending information to server PC.
So, I recommended to UIA to capture data in the target board, and send it to server PC through Ethernet, and open it in the CCS when needed.
in this scenario, my questions are
1. do you think this is realistic scenario?
2. Is it possible to detect UIA data in the server PC if it is mixed with other data? could you please share the example code or how it can be detected?
3. Is there any example code for server PC? LoggerSM is good examples on this? or is there any other example code?
4. How UIA data stored in the server PC? e.g. what is the file format should be used in the server PC(host) storage and open it in CCSv6?
Thanks and Best Regards,
SI.