The stability of which power rail, CVDD or DVDD, is critical to the stability of the PLL at high multiplication ratios in the TMS320CV5509? If they both have a role which is the more significant?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The stability of which power rail, CVDD or DVDD, is critical to the stability of the PLL at high multiplication ratios in the TMS320CV5509? If they both have a role which is the more significant?
Hi,
As per "SPRAA30" CVDD power supply looks critical. Here is the reference from TMS320VC5509A Hardware Designer’s Resource Guide
" The digital PLL (DPLL) used to provide clock to the DSP is sensitive to the quality of the power supply. Excessive power supply ripple can contribute to excessive clock edge jitter on the DPLL. CVdd power supply ripple of less than 20 mV is recommended for optimal DPLL jitter performance".
Hope this information helps.
Regards
Vasanth