Other Parts Discussed in Thread: AM5728
Hi,
I have one question regarding TI wiki of AM572x.
According to TI Wiki (http://processors.wiki.ti.com/index.php/AM572x_Schematic_Checklist ) , it is written in the below.
If RTC feature is not used,
RTC_ISO pin should be connected to PORZ.
RTC_PORZ pin should be connected to VSS.
However, according to the AM5728 data manual "Table 4-1. Unused Balls Specific Connection Requirements", it is written in the below.
AF14(rtc_iso) must be connect to the corresponding power supply through an external pull resister if unused.
AB17(rtc_porz) must be connected to F22(porz) if unused.
Which is correct, checklist ? or data manual?
Please advise me.
I appreciate your quick reply.
Best regards,
Michi