This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C Test: 400Kbps: Data Mismatch

Greetings...

I have followed the directions from the page 

"processors.wiki.ti.com/.../Processor_SDK_RTOS_Creating_a_SD_Card_with_Windows

The contents of the SD were the two files that I expected. However, when I try to boot the AM335X Starter Kit I get the following...

I2C Test: 100Kbps:Data Mismatch

Some tests have failed.

StarterWare Boot Loader
BOARDInit status [0x0]
SoC : [AM335X]
Core : [A8]
Board Detected : [EVMSK]
Base Board Revision : [1.2B]
Daughter Card Revision: [UNKNOWN]
GPIO Instance number: 0
Pin number: 7
Copying application image from MMC/SD card to RAM
Jumping to StarterWare Application...


I2C Test: 400Kbps: Data Mismatch

I2C Test: 100Kbps:Data Mismatch

Some tests have failed.

Can someone please help an old dude out?

VR/JW