Hi.
We use the IBL NAND boot options in TMDSEVM6678L board.
Place the two written in NAND applications, there is a problem in attempting to use by selecting according to the boot option.
Boot option IBL NAND boot on image 0 is normal, IBL NAND boot on image 1 does not execute the application
In iblNandBoot function it does not execute a jump to the address written on the NAND. (In the IBL NAND boot on image 1)
Is there anything in addition to selecting the boot mode you need more? Advice please.