Other Parts Discussed in Thread: TLV320AIC3204
Hi,
I need multiple audio sources and multiple outputs, so I am thinking of using the expansion slot of the C5505 eZdsp USB stick to interface another TLV320AIC3204 codec.
I will use the DSP's I2S2 interface (pins 19, 21, 23 & 25 on the expansion header) to map the I2S pins of the 2nd AIC3204 codec, but how will I handle the I2C communication b/w the DSP and the 2nd codec ?
Won't I end up with two devices (TLV320AIC3204 codecs) having the same slave address ?
If YES, please help me out in achieving a control interface between the DSP and the 2nd TLV320AIC3204 codec...
Thank you,
Bhargav