This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dm8168 nfs booting stuck

Hi:

I've made a board with dm8168 myself, but it can't booting normally,

always gets stucked at booting as fellowing:

 Waiting 10sec before mounting  root device...

PHY: 0:01 - Link is Up - 1000 /Full

VFS: Mounted root (nfs filesystem) on device 0:15.

Freeing init memory: 228K

INIT: version 2.88 booting

Then,it stucked here.

plus,I've test my bootargs and uImge,filesystem on TI' evm board, which work well.

so,I doulted if any parts of my HW got problems, or anything else?

would anyone help me out ?

Thanks a  lot!