This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L137 EVM bootloader

Other Parts Discussed in Thread: OMAP-L137

Hello, I have a basic question about OMAP L137 EVM boot loader.  On the Technical Reference, it says EVM key features include “SPI Boot EEPROM”.  However, I look at the setup of the SW2 Boot Mode Selection.  It is SPI0 Flash.  Is it a mistake of the manual?  I think it does boot from SPI0 flash, instead of EEPROM.  Also, it seems like the actual codes are stored on the SD card.  Does the EVM boot from SPI0 flash, then switch to the SD card to execute the actual codes?