This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Playing with pulseaudio on Vayu EVM

Hi,

I am trying to play using Pulseaudio on Vayu EVM with GLSDK 7.03.

root@dra7xx-evm:/media# pulseaudio --system& 
root@dra7xx-evm:/media# Running in system mode, but --disallow-exit not set! i
root@dra7xx-evm:/media# Running in system mode, but --disallow-module-loading not set! o
root@dra7xx-evm:/media# Running in system mode, forcibly disabling SHM mode! c
root@dra7xx-evm:/media# Running in system mode, forcibly disabling exit idle time! o
root@dra7xx-evm:/media# W: [pulseaudio] main.c: OK, so you are running PA in system mode. Please note that you n
root@dra7xx-evm:/media# If you do it nonetheless then it's your own fault if things don't work as expected. v
root@dra7xx-evm:/media# Please read pulseaudio.org/.../WhatIsWrongWithSystemMode for an explanation whye
root@dra7xx-evm:/media# Daemon startup without any loaded modules, refusing to work.

paplay file.wav just hangs, but no sound heard from headphone, though aplay works.

Could you please help me to get paplay working. My final target is to measure playback and recording latency. I heard that latency can be lower if one uses pulseaudio instead of ALSA directly.

Thanks in advance,

Parag