Other Parts Discussed in Thread: SYSBIOS
Hello all,
WHen running a load of software on a C6678 with SYS/BIOS 6.32.5.54, some time after startup (sometimes immediately, sometimes after around 10 minutes of normal operation) I receive an Instruction Fetch Exception error and my code exits. The data that is printed to the console is the following:
B13=0x0
B14=0x86a838 B15=0xc26bd58
B16=0xc268df0 B17=0x0
B18=0x2e30000[C66xx_8] B19=0x0
B20=0x0 B21=0x2e3
B22=0x2e30000 B23=0x0
B24=0x0 B25=0x3000
B26=0x3000 B27=0x0
B28=0x0 B29=0x3
B30=0x640 B31=0x1dcd696e
NTSR=0x1000f
ITSR=0xf
IRP=0x84ad20
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x1bc94f6
EFR=0x2 NRP=0x1bc94f6
Internal except[C66xx_8] ion: IERR=0x1
Instruction fetch exception
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x0084ad20, sp = 0x0c26bd58.
xdc.runtime.Error.raise: terminating execution
In searching for this issue on other posts, I opened up the ROV and looked through the exception handler. The B3 register stored in the exception is set to 0x00849260, which when looking through the disassembly this address maps to an instruction set labeled $C$RL1. When examining the disassembly given for NRP, the actual address is a NOP operation, and everything surround it is alternating NOP and SWBP instructions.
I imagine this is a memory issue somewhere, where a pointer is getting trashed somewhere, but I am having a difficult time tracking down the root cause. In looking at my Tasks in the ROV nothing appears to be blowing its stack, at least there are no notifications of such and all of the peaks given are below the sizes. Similarly, HeapMem size given appears to have plenty of free size, and the HWI module has a stack much larger than it's given peak.
As an additional note, I am sometimes receiving Double Free exceptions occurring instead of the exception above, although the code is not completing and free operations, far as I can tell.
I think that's about all of the information I have on it; if anyone has any suggestions on what might be causing this or avenues to approach, I would be greatly appreciative.