Dears
use ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install.bin SDK
When put finger on touch than echo mem > /sys/power/state to power standby mode at the same time that resume than touch panel position error.
Because customer they AP do power standby mode in 2-3 sec that end user to touch at the same time so customer AP will ignore the status.
The system will go power standby mode and resume .Maybe can happen touch panel position error.
PM: Syncing filesystems ... done.
[ 138.607188] Freezing user space processes ... (elapsed 0.001 seconds) done.
[ 138.615630] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
[ 138.624401] Suspending console(s) (use no_console_suspend to debug)
[ 138.750157] PM: suspend of devices complete after 118.475 msecs
[ 138.751614] PM: late suspend of devices complete after 1.420 msecs
[ 138.756566] omap_hwmod: adc_tsc: _wait_target_disable failed
[ 138.757289] PM: noirq suspend of devices complete after 5.639 msecs
[ 138.757448] PM: Successfully put all powerdomains to target state
[ 138.757448] PM: Wakeup source UART
[ 138.790229] PM: noirq resume of devices complete after 32.683 msecs
[ 138.791732] PM: early resume of devices complete after 1.067 msecs
[ 138.792762] net eth0: initializing cpsw version 1.12 (0)
[ 138.870373] net eth0: phy found : id is : 0x4dd074
[ 138.870505] libphy: PHY 4a101000.mdio:01 not found
[ 138.870525] net eth0: phy 4a101000.mdio:01 not found on slave 1
[ 139.219810] PM: resume of devices complete after 428.019 msecs
[ 139.294543] Restarting tasks ... done.