Other Parts Discussed in Thread: AM3358
Hi Guys,
For am3358 starter kit.
1, from the AM3358 starter kit schematics, the RGMII2_INT and RGMII1_INT pins from two AR8031 is connected to USB1_DRVVBUS and GPIO1_28 of AM3358.
2, From TI WIKI
processors.wiki.ti.com/.../AM335xStarterKitHardwareUsersGuide
.The interrupts from the both PHYs are connected to both the Non Maskable Interrupt pin and to the processor GPIO pins
but I can't find the GRMII2_INT and RGMII1_INT setting for PHY interrupt in uboot and kernel.
My question is :
GRMII2_INT and RGMII1_INT is not be used in uboot and Kernel ?
thanks!