I have to record a video and store each frame into the processor. Can you please help me get started with this project
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have to record a video and store each frame into the processor. Can you please help me get started with this project
Hi,
Thanks for your post.
It would be a good start to experiment BSL examples and you could download the same from the below board manufacturer's link:
http://c6000.spectrumdigital.com/evmdm642/V3/docs/bsp/index.html
It would be good that you could try LED blinking, tone generation and audio processing examples. Also, there are example tests, gel files, BSL and download the BSL test example zip file from the below :
http://c6000.spectrumdigital.com/evmdm642/
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------