Hi,
I would need the OMAP3530 pin list in an excel format (table 2-4 of the omap3530 datasheet)
Is it available somewhere?
Thanks
Philippe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Philippe:
The Pin Mux Utility for ARM MPU Microprocessors v1.0.1.0 is now available via the AM3715 and AM3703 product pages. Go to "Tools and Software", then "PinMux Utility for Sitara Devices", then "Get Software". You should see one file to download named "Pin_Mux_Utility_v1_00_01_00". This supports AM37xx, AM35xx and OMAP35xx devices.
Best Regards,
Mike Tadyshak
ARM MPU SW Applications Engr.