Other Parts Discussed in Thread: OMAP3530, OMAP3525, DM3725
Hi,
Has anyone designed a circuit with OMAP3530 and Strataflash (NOR Flash) memories?
I would then need to use the multiplexed address/data output, but the flash has separate address and data input ports.
If I connect A[1..16] (flash side) in parallel with D[0..15], I am afraid because of the max.load of 15.94pF stated in table 6-2 of the datasheet.
My memory device has a max.load of 9pf per pin, so two in parallel are already exceeding the max.load of the omap, without counting pcb...
I need to know if this configuration would work in practice, and at what performance.
Thanks
Philippe