Other Parts Discussed in Thread: AM3357
I want to add I2C2 to uboot and test the i2C2 in uboot level. how to add i2c mux configuration in uboot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3357
I want to add I2C2 to uboot and test the i2C2 in uboot level. how to add i2c mux configuration in uboot.
Hi,
You should:
- add static struct module_pin_mux i2c2_pin_mux[] in board/ti/am335x/mux.c
- in boar/ti/am335x/mux.c add:
void enable_i2c2_pin_mux(void)
{
configure_module_pin_mux(i2c2_pin_mux);
}
- call configure_module_pin_mux(i2c2_pin_mux) again in board/ti/am335x/mux.c
- in const struct dpll_params *get_dpll_ddr_params(void) in board/ti/am335x/board.c add:
enable_i2c2_pin_mux();
i2c_init(<i2c2 speed>, <i2c2 slave>);
In include/configs/ti_armv7_common.h, add i2c2 slave & i2c2 speed (used above):
#define CONFIG_SYS_OMAP24_I2C_SPEED 100000
#define CONFIG_SYS_OMAP24_I2C_SLAVE1 2
This should enable your i2c2 controller.
Best Regards,
Yordan
Dear Yordon,
thanks for u r reply,,,,,,,,,,
i have struck with another error after booting my custom board i entered the usb command like "lsusb" it showing the below error..........
"unable to initialize libusb: -99"
i am attaching my log information.........
Hi, I don't understand how this function tell that we need to init the bus 2:
i2c_init(<i2c2 speed>, <i2c2 slave>);
In this function it get the bus number with i2c_get_bus_num() but to define a bus number, you have to call before i2c_set_bus_num(unsigned int bus).
what is slaveAddr ? the address of a device ?
I'm trying to use I2C2 instead of I2C0 ... but it doesn't work.
I've put some trace in the function i2c_get_adapter and it's always index 0. So I'm assuming that it's I2C0 that it is used.