Hey,
I would like to find explanation for the following issue. I am using the TI RTOS (2.16.0.08) Wifi example for TivaC launchpad. (tcpEchoCC3X00_EK_TM4C123GXL_TI_TivaTM4C123GH6PM) I did everything that the readme suggested and I could successfully configure and connect my LP to the home wifi network.
My problem is when I restart the LP it can not connect to the home wifi every time when I restart it. No IP displayed on the Console, and the RGB led doesn't change the color from blue only several times. I increased the time btw restarts but nothing changes.
The distance btw the LP and wifi router (TL-WDR3600) is less than 5 meters.
Have you faced similar issue like this one? Looking forward any reply.
Thank you