Hi All.
This is Masaharu Takahashi in Japan.
Could you tell me as below question?
[DM6446 USB2.0 High-Speed BulkIN Transaction.]
At my customer's system, DM6446 USB2.0 are used as High-Speed device(peripheral).
It is connected to Host PC(USB Host) and they are having problem during BulkIN transaction.
(This system is non-OS)
While USB communication are working fine,
sometimes DM6446 USB won't send any response(DATA/NACK/STALL) after IN Token send from the Host USB.
And Host USB keep sending IN Token 3 times continuously whether USB device(DM6446) are not sending response.
After Host sending IN Token 3 times as above, Host are sending next SOF,
and it seems Bulk Transaction are woriking fine again.
What kind of things will cause this issue?
question 2.
[USB Revision]
Could you tell me what is USB Revision for DM6446BZWT as well OMAP L137 ?
Thanks,
Best Regards,
Masaharu Takahashi