Hi TI's experts
We are working on DaVinci Processor DM8148 McASP now .
there is a input data timing like this :
the slot is 32bit , left and right channel just like IIS timing .
but there is only 16bit real data like below :
NNNN-NNNN-DDDD-DDDD-DDDD-DDDD-NNNN-NNNN
we can not change the slot size which is 32bit width , so can we use the XFMT register to modify the McASP receive this type timing ?
Slot size is 32bit
Data size is 16bit
but how to set the register to ignore the first 8 bit data ? and capture the 16bit real data to the linux user space ?