Is a Low Voltage Adaper required to use XDS510 (TI Part # TMDSEMU510U) with the OMAP3530? Initially working with the IGEPV2 board sold by the Spanish company ISEE.
The Spectrum Digital Technical Reference for the XDS510 (dated 2005) talks about the low voltage adapter in two places.
It says that the XDS510 supports 3.3 and 5.0 volt (3.3 to 1.8 with Low Voltage Adapter).
Then section 2.3 of the document is an entire section on the proper installation of the Low Voltage Adapter part #701208. But, no where in the document does it give a hint as to whether this adapter board is included with the emulator or sold separately. Is there a separate part number for the adapter?
Thanks.