Hi,
I confirm it in the following environment.
Device:AM437x
Customer board
EVM board
A problem occurs with both.
The following errors occur when they copy data of 20MB continually in USB memory.
[130.161429] is Cannot enable port 1 1.0 hub 1-0. Maybe the USB cable is bad?
[134.271404] is Cannot enable port 1 1.0 hub 1-0. Maybe the USB cable is bad?
[138.381427] is Cannot enable port 1 1.0 hub 1-0. Maybe the USB cable is bad?
[142.491418] is Cannot enable port 1 1.0 hub 1-0. Maybe the USB cable is bad?
Please tell me the factor that this error occurs.
There is dependence in the memory of the USB, and there is the thing which the problem does not occurs or the problem occurs.
Problem USB memory:
IO-DATA:BUM-3B8G/K
USB memory without the problem:
BUFFALO:RUF2-K8GR
SONY: USM4GR
There is following difference in even problem USB memory by the version of SDK.
SDK version Result
AM437xSDK08_00_00_00 GOOD
PROCESSOR-SDK-LINUX-AM437X01_00_00_00 GOOD
PROCESSOR-SDK-LINUX-AM437X01_00_00_03 BAD
PROCESSOR-SDK-LINUX-AM437X02_00_00_00 BAD
PROCESSOR-SDK-LINUX-AM437X02_00_01_07 BAD
PROCESSOR-SDK-LINUX-AM437X02_00_02_11 BAD
From the result mentioned above, will there be any information?
Best Regards,
Shigehiro Tsuda